{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Video: Where can wiring diagrams be found for the local and remote Safe/ Hazard alarms IG2000CBM , IG2000PG1, IG2000PG2, IG2000PPM used with Isolation panels?
Issue:
Where can wiring diagrams be found for the local and remote Safe/ Hazard alarms used with Isolation Power Panels?

Product Line:
Medical Products 
Isolated Power System

Environment:
Iso-Gard™ Isolation Panel Alarms & Indicators

Cause:
Wiring reference

Resolution:
See attachments for wiring diagrams and connecting the Iso-Gard™ IG2000CBM remote indicator to an Iso-Gard™ Series 6 (IG6) line isolation monitor's connection plate .

Schneider Electric USA

Attachment(s)
IG2000CBM.pdf [603.33 KB]
IG2000PG1.pdf [135.33 KB]
IG2000PPM.PDF.pdf [74.03 KB]
IG6 SET_UP_ERROR8.80_2-12.pdf [278.33 KB]
IG6 Instruction Bulletin for (Series 6 LIM) MED10110103.pdf [841.46 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range: