{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Can the sub feed lug kit SL800M5 be change from accommodating (3) 3/0 - 500kcmill to (4) 3/0- 500 kcmil wire used with an ILine 800A MCB Panelboard ?
Issue:
Can the sub feed lug kit SL800M5 be change from accommodating (3) 3/0 - 500kcmill to (4) 3/0- 500 kcmil wire used with an ILine 800A MCB Panelboard ?

Product Line:
I Line Panelboard accessories

Environment:
Application

Cause:
Product Features

Resolution:
Due to the 800A rating of the sub feed lug kit , there is no provisions, or wire bending space for the SL800 , used with a HCM , or HCP interior to run (4) 500 kcmil/ phase .
Using a HCRU interior with back fed PG 1200AF/800AT breaker, or SL1200P5 Sub feed lug kit , will offer (4) 3/0-500 kcmil/phase

Schneider Electric USA