{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Can the standard 2 pole QO or Homeline Circuit breaker be used to feed (2) 120 V Circuits?
Issue:
Can the HOM230 be used to feed (2) 120V circuits?

Product Line:
Miniature Circuit breaker

Resolution:
​Yes, these breakers can serve two circuits. Keep in mind that since they are 2 pole breakers, they have common trip, which means if there is a fault in one of the poles, both of them would trip.

Schneider Electric USA