{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Can a 3p QO-GFI breaker be used on a load with no load neutral?
Issue:
Can the 3-pole QO-GFI breakers work without a load neutral connected?

Product Line:
QO Branch Breakers

Resolution:
Yes, the 3p QO-GFI breakers can ONLY be used on loads without a neutral. There is not a spot to connect a load neutral on the breaker, and a load neutral for the circuit connected to the neutral bar will cause nuisance tripping.

Schneider Electric USA