{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
How to install 9999AC04 auxiliary contact to a 9065 SSOLR?

Article available in these languages: Spanish

Issue:
What are the steps installing 9999AC04 in a SSOLR?

Product Line:
NEMA Starters and Contactors

Environment:
NEMA Starters and Contactors accessories

Resolution:
When adding the additional (and optional) auxiliary contact to a SSOLR relay (standard or feature base), it is necessary to remove the dust shield from the top of the overload relay.  The dust shield covers up the access holes required to install the Class 9999 Type AC04 auxiliary contact module.
It is shaped similar to a large pair of square glasses and is cemented down.  You have to use your fingernail or a small utility knife to pull the dust shield up off the plastic case of the overload relay.

Schneider Electric USA

Attachment(s)
9999AC04 - Contact Dust Cover Removal_.pdf [25.38 KB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: