{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Can you install a LSIG main breaker in I line distribution using NEMA 4X enclosure?
Issue:
Are there any restrictions for having a LSIG main breaker for I line panel in NEMA 4X enclosure?

Product Line:
Panelboard

Environment:
Square D I-line panelboard

Cause:
Application

Resolution:
LSIG main breaker requires a neutral CT and power supply. These neutral CT's and power supplies require a side extension which is not an option for NEMA 3R or 4X enclosures. Since NEMA 4X is factory assembled and needs to be built in product selectors, an error message "Change enclosure Type to Type 1- Gutter extensions are not available in non-ventilated enclosures" will appear.

Schneider Electric USA