{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Is the impedance 3.1% for EE50S3HBCU still accurate? This is referencing and based on data bulletin 7400DB0702R07/09?
Issue:
What is the Impedance for a EE50S3HBCU transformer?

Product Line:
LV Transformer

Environment:
Application

Cause:
Product Features

Resolution:
The current designed EE50S3HBCU transformer and information in the 7400DB0702R07/09 Bulletin, page 10, Table 10, see attached , are correctly represented by an Impedance IZ =  to 3.1%

Schneider Electric USA

Attachment(s)
EE50S3HBCU Performance Data.pdf [24.4 KB]