{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the Degree of Protection of the 9001K and 9001SK Operators?
Issue:
Looking for information on the NEMA rating for the 9001K and 9001SK operators

Product Line:
Harmony 30 mm Push Buttons

Environment:
Push Buttons and Operator Interface

Resolution:
The 9001SK operators are rated NEMA 1, 2, 3, 3R, 4, 4X, 12, 13.
The 9001K operators are rated NEMA 1, 2, 3, 3R, 4, 12, 13.

Schneider Electric USA