Issue:
What are the breakdown parts that make up a LK4JUKB1 kit?
Product line:
Motor switch-disconnectors and fuses
Environment:
TeSys LK4 Non fusible disconnect switches
Resolution:
LK4JUKB1 - BLACK - NEMA 1, 12, 3R
What are the breakdown parts that make up a LK4JUKB1 kit?
Product line:
Motor switch-disconnectors and fuses
Environment:
TeSys LK4 Non fusible disconnect switches
Resolution:
LK4JUKB1 - BLACK - NEMA 1, 12, 3R
Unit is only sold as a kit made up of the following parts:
LK4JU3CN - 30A Switch
LK4AE41CN - 400mm Shaft
LK4AH0110C - Black Handle NEMA 1, 12, 3R
GS2AEH12 - Guide Cone
It is very important that these new shafts and handles are mounted according to the instructions provided with the new components. The new handles REQUIRE drilling new holes for mounting. Using the new handle in mounting holes from an older unit wil break the switch. Reference 30072-454-20A attached.
Released for:Schneider Electric USA