{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Do the GV3 starters have de-rating based on ambient temperatures?
Issue:
Customer wants to use the GV3 starter in ambient temperature of 50C.  Asking for de-rating information.

Product line:
Contactors and Starters-IEC

Environment:
Tesys GV

Cause:
Catalog does not show temperature de-rating info.

Resolution:
The GV3P can operate from -20 to +60C in open spaces or -20 to +40C in enclosures without derating because they have a temperature compensation system.

The temperature limitation for enclosures is due to air circulation around the product being limited.  No derating is available above or below this temperature range.

Schneider Electric USA