{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the firmware version of Micrologic 3.2 and 3.3 Trip Units?
Issue:
Do Micrologic 3.2 and 3.3 trip units have firmware?

Product Line:
Circuit Breakers

Environment:
Applies to breakers with suffix U31X or U33X, which have Micrologic 3.2 or 3.3 trip units

Resolution:
The Micrologic 3.2 and 3.3 Trip Units do not have firmware. They are a standard trip unit with only an ASIC (Application-Specific Integrated Circuit) which is hard-coded.

Schneider Electric USA

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: