Issue:
Can a SDSA2040 Surge Protective Devices be used on ANY Competitor's panelboard, or load center?
Product Line:
Surge Protective Devices
Environment:
Application
Cause:
Installation
Resolution:
The Catalog number SDSA2040 Secondary Surge Arrester (SPD) CAN be used on any 3-Phase / 4 wire, 208Y/120 V, Panelboard or load center.
Can a SDSA2040 Surge Protective Devices be used on ANY Competitor's panelboard, or load center?
Product Line:
Surge Protective Devices
Environment:
Application
Cause:
Installation
Resolution:
The Catalog number SDSA2040 Secondary Surge Arrester (SPD) CAN be used on any 3-Phase / 4 wire, 208Y/120 V, Panelboard or load center.
Released for:Schneider Electric USA
Issue:
Can a SDSA2040 Surge Protective Devices be used on ANY Competitor's panelboard, or load center?
Product Line:
Surge Protective Devices
Environment:
Application
Cause:
Installation
Resolution:
The Catalog number SDSA2040 Secondary Surge Arrester (SPD) CAN be used on any 3-Phase / 4 wire, 208Y/120 V, Panelboard or load center.
Can a SDSA2040 Surge Protective Devices be used on ANY Competitor's panelboard, or load center?
Product Line:
Surge Protective Devices
Environment:
Application
Cause:
Installation
Resolution:
The Catalog number SDSA2040 Secondary Surge Arrester (SPD) CAN be used on any 3-Phase / 4 wire, 208Y/120 V, Panelboard or load center.
Released for:Schneider Electric USA