{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Can I Line Busway be used with 480V and 208V busway together?
Issue:
Is there a way to combine 2 different voltages to the same piece of I Line II Busway?

Product Line:
I Line II Busway

Environment:
Application

Cause:
Product Features

Resolution:
I Line II Busway is rated for 3P/3W , or 3P/4W Voltage systems up to 600V\. The Plug on Switches are listed with fusing for 240, or 600V and only one voltage system can be used thru the same run of Busway

Schneider Electric USA