{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Video: How to wire a PowerPacT P frame or R frame shunt trip or undervoltage trip
Issue:
Wiring Shunt or Undervoltage Trip on PowerPact P & R-Frame Circuit Breakers

Product Line:
Molded Case Circuit Breaker Accessories

Resolution:
Once the shunt or under voltage is installed, install the provided termination block in the hole located directly above the handle of the breaker. You will slide the connector from the shunt or under voltage into the termination block. The control wiring would then be lead into the two terminal screws on the termination block. For more information, see the video below:

Schneider Electric USA