Issue:
What are the part numbers for the handle and shaft that can be used on the old LK3QU3 switches?
Product line:
IEC Disconnects
Environment:
LK3
Resolution:
Use the GS2AE61 (15.7" shaft) and GS2AH150 for black handle and GS2AH160 for red/yellow handle. Will also need the GS2AH100TO200 adapter for the handle. Both handles are rated Nema 4/4X
Both handle and shaft needs to be replaced.
What are the part numbers for the handle and shaft that can be used on the old LK3QU3 switches?
Product line:
IEC Disconnects
Environment:
LK3
Resolution:
Use the GS2AE61 (15.7" shaft) and GS2AH150 for black handle and GS2AH160 for red/yellow handle. Will also need the GS2AH100TO200 adapter for the handle. Both handles are rated Nema 4/4X
Both handle and shaft needs to be replaced.