{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Will the Peak Menu Max amperage function capture the maximum amperage of a short circuit?
Issue:
What is the purpose of the max amperage current function (Imax)?

Product Line:
Circuit Breakers

Environment:
Micrologic trip units found on Powerpact H,J,L,P,R frame and Masterpact NT/NW  Display: peak current, or Max current display value
Models: 2.0A, 3.0A, 5.0A and 6.0A, 5.0P, 6.0P, 5.0H, 6.0H, 5.2A,5.3A, 6.2A,6.3A, 5.2E,5.3E,6.2E and 6.3E

Resolution:
The peak or max current function is only for load currents and overloads and slowly rising ground faults.  This function is not meant to capture the maximum current during a short circuit.

Schneider Electric USA