Search FAQs
Model 6 MCC: Will the 30mm operators fit in the 22mm holes?
Issue:
How to replace 22 mm operators, in a Model 6 Motor control center, with 30MM operators?
Product Line:
MCC or Motor Control Center
Environment:
Model 6
Cause:
N/A
Resolution:
The best option is to replace the 22 mm control plate with the 30 mm control plate. The part number is 80420-007-06. This can be obtained from the local distributor. The other option is to use a 30 mm knockout tool.
How to replace 22 mm operators, in a Model 6 Motor control center, with 30MM operators?
Product Line:
MCC or Motor Control Center
Environment:
Model 6
Cause:
N/A
Resolution:
The best option is to replace the 22 mm control plate with the 30 mm control plate. The part number is 80420-007-06. This can be obtained from the local distributor. The other option is to use a 30 mm knockout tool.
Released for:Schneider Electric USA
Explore more
Range:
Explore more
Range: