{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Is there a way to deactivate the Unity Pro DTM audit tool?
No. When you import a project that contains DTMs that are missing or incompatible (not reverse compatible as well) the audit tool opens and provides the necessary information.

***** As of Control Expert v15.3 there is a 'do not show this message for backwards compatibility' checkbox that can be selected when the audit tool first appears. *****

There is no method to stop the tool from reporting on the other flagged problem DTMs when opening projects as this is important information.

Schneider Electric USA