How can we help you today?
Can a shunt trip accessory be added to ANY of the EZM main breaker devices?
Issue:
Product Design Features
Product Line:
EZM Metering
Resolution:
Yes, a shunt trip can be added to the main breakers used in all of the current EZM main breaker devices. Some older devices used breakers that would not accept field installable accessories.
To get a Shunt trip, it will require one to go to the current CAD drawing for the EZM Main catalog number and determine what Breaker is used in that EZM Main, then obtain the shunt trip for that breaker.
NOTE: The Shunt Trips for the EZM Main Devices can ONLY be field installed, there are NO factory installed options.
Product Design Features
Product Line:
EZM Metering
Resolution:
Yes, a shunt trip can be added to the main breakers used in all of the current EZM main breaker devices. Some older devices used breakers that would not accept field installable accessories.
To get a Shunt trip, it will require one to go to the current CAD drawing for the EZM Main catalog number and determine what Breaker is used in that EZM Main, then obtain the shunt trip for that breaker.
NOTE: The Shunt Trips for the EZM Main Devices can ONLY be field installed, there are NO factory installed options.
Released for:Schneider Electric USA
Explore more
Category:
Explore more
Category: