Issue:
Using the AT1PA2 crimp tool, asking for the specifications on the pull out strength needed to remove the cable from the cable end.
Product line:
DZ5 cable end
Environment:
Terminal Blocks
Resolution:
We do not have the crimp force applied using the AT1PA2 crimp tool. The DZ5CE cable ends meet the testing requirements for standard IEC 60947-1, table 5.
Using the AT1PA2 crimp tool, asking for the specifications on the pull out strength needed to remove the cable from the cable end.
Product line:
DZ5 cable end
Environment:
Terminal Blocks
Resolution:
We do not have the crimp force applied using the AT1PA2 crimp tool. The DZ5CE cable ends meet the testing requirements for standard IEC 60947-1, table 5.
Released for:Schneider Electric USA