{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Video: Demonstrating acceptable installed QO branch breaker movement
Issue:
What type of movement does a QO branch breaker have once installed with and without the deadfront/cover installed?

Product Line:
QO Load Centers & Circuit Breakers

Resolution:
Once a QO branch breaker is installed on the interior of a QO load center, there will be some small amount of movement of the breakers before the deadfront/cover gets installed. Then, as more branch breakers get installed next to each other, the movement will become less. Once the deadfront/cover is installed, the movement of the branch breakers will be lessen further.

Schneider Electric USA