{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.

How can we help you today?

Video: Where is the actual catalog number, series number and wiring schematic located on the Meter-Pak device?

Issue:
Finding the catalog number, series number and wiring schematic on MP Meter-Pak Meter Center devices.

Product Line:
Meter Pak Metering

Resolution:
The actual catalog and series number, along with the wiring schematic and other general information about the Meter-Pak devices, will be located on the wiring diagram label, which is located on the back side of the tenant breaker compartment cover.

NOTE: To actually see the wiring diagram label, it requires the front tenant breaker compartment cover to be REMOVED from the device.
SEE BELOW A VISUAL OF A METER-PAK DEVICE WIRING DIAGRAM LABEL. ALSO SEE BELOW A VIDEO.

THE BELOW IS ONLY A SAMPLE LABEL, THE LABEL THAT COMES ON THE PARTICULAR DEVICE WILL CONTAIN INFORMATION SPECIFIC TO THAT DEVICE.

Label example

Schneider Electric USA