Search FAQs
Are any QO or Homeline load centers available with feed-through lugs?
Issue:
Product Design Features
Product Line:
QO and Homeline Load Centers
Resolution:
There are only a few QO and Homeline load center catalog numbers that come with feed-through lugs. Only the catalog numbers with the suffix FT in the number are supplied with feed-through lugs.
NOTE: Load centers CANNOT be modified in the field to add feed-through lugs.
The QO catalog numbers available are:
QO1612M125FTRB
QO1816M150FTRB
QO1816M200FTRB
The Homeline catalog numbers available are:
HOM816M150PFTRB
HOM816M200PFTRB
Product Design Features
Product Line:
QO and Homeline Load Centers
Resolution:
There are only a few QO and Homeline load center catalog numbers that come with feed-through lugs. Only the catalog numbers with the suffix FT in the number are supplied with feed-through lugs.
NOTE: Load centers CANNOT be modified in the field to add feed-through lugs.
The QO catalog numbers available are:
QO1612M125FTRB
QO1816M150FTRB
QO1816M200FTRB
The Homeline catalog numbers available are:
HOM816M150PFTRB
HOM816M200PFTRB
Released for:Schneider Electric USA
Explore more
Range:
Category:
Explore more
Range:
Category: