{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
M580 Hot Standby automatic IP address swapping.

Article available in these languages: Spanish

Issue
How is the M580 Hot Standby IP address swapping feature configured using Unity Pro?

Product line
Control Expert, Unity Pro, Modicon M580

Resolution
The addressing swapping feature is not something that can be turned on and off. It is not configurable. When you have synchronized M580s both online, the Primary will have the Main IP and the Standby will have the Main IP +1. If the Primary fails, the formerly Standby will become Primary and inherit the Main IP address.

Schneider Electric USA