Search FAQs
Will HOM-DF (dual function) breakers with a pigtail work on HOM24L70F, HOM24L70S, and HOM24L70RB load centers?
Issue:
Can the HOM-DF breakers be installed on HOM24L70 series load centers?
Product Line:
Load Center
Resolution:
No. The pigtail HOM-DF breakers are for use in all Homeline load centers EXCEPT all versions of HOM24L70. The plug-on neutral version will also not install as this load center is not plug-on neutral ready. See attached instruction bulletin HRB86114 as reference.
Can the HOM-DF breakers be installed on HOM24L70 series load centers?
Product Line:
Load Center
Resolution:
No. The pigtail HOM-DF breakers are for use in all Homeline load centers EXCEPT all versions of HOM24L70. The plug-on neutral version will also not install as this load center is not plug-on neutral ready. See attached instruction bulletin HRB86114 as reference.
Released for:Schneider Electric USA
Attachment(s)
Explore more
Range:
Explore more
Range: