{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What do the suffixes EA, EB, EG, EH, EK, and EL mean in PowerPacT H, J, and L frame circuit breakers?
Issue:
Meaning of the EA, EB, EG, EH, EK and EL suffixes for PowerPacT circuit breakers

Product Line:
Molded Case Circuit Breaker

Resolution:
EA = Factory installed 1.3 m (4.27 ft) NSX Cord 
EB = Factory installed 3 m (9.84 ft) NSX Cord 
EG = Factory installed 1.3 m (4.27 ft) BSCM (breaker status and control module) with NSX Cord
EH = Factory installed 3 m (9.84 ft) BSCM with NSX Cord
EK = Factory installed 1.3 m (4.27 ft) BSCM with NSX Cord for V > 480 Vac
EL = Factory installed 3 m (9.84 ft) BSCM with NSX Cord for V > 480 Vac

Schneider Electric USA

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
move-arrow-top