{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
How Many spaces does a NB3P100 take up in a FPE NBLP or NBDP panel?
Issue:
Does the NB3P100 require more than 3 spaces to mount in a panelboard?

Product Line:
Panelboards

Resolution:
The NB3P100 takes up a total of 6 spaces in a Federal Pioneer NBLP or NBDP panelboard.
This is also true for the NB3P90. No breakers can be mounted opposite these breakers in the panel.

Schneider Electric USA