{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Can you add a QO2200 branch breaker into a NQ panelboard?
 Issue:
Can a QO2200 (or QO2150 or QO2175) be used in an NQ panelboard?

Product Line:
NQ Panelboards

Resolution:
No, this breaker is not CSA listed or warranted for application in an NQ panelboard.
THIS BREAKER IS FOR USE IN SINGLE PHASE QO LOAD CENTERS ONLY.
 
To get a 200A Branch breaker in an NQ panelboards, you have to use a Sub feed breaker kit, and increase size of box and trim.

Schneider Electric USA

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: