{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What does "PLR" suffix means for enclosure part number HC4486DBPLR ?
Issue:
When an I-Line NEMA 1 enclosure is ordered with a "PLR" suffix what does it include?

Product Line:
I-Line Panelboard

Environment:
Product Features

Resolution:
The "PLR" suffix represents a 14" auxiliary section bolted to the right side of a standard 44" Wide I line HCRU box.  It has s separate 14" wide by 9.5" deep endwall.  The side walls are open between the two sections except for an approx. 1.5" flange all around.
The panel is designed for conduit entry for the standard 44" Wide box area only. However, the Contractor can enter the box anywhere he chooses as long as it is acceptable to the local inspector.
HC4486DBPLR is a special part number, this will require contacting a local distributor who will then work with the local sales office to order it.

Schneider Electric USA

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: