{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the Ambient Temperature rating for the MTZ breaker?
Issue:
Is there a minimum and maximum operating temperature for the MTZ breaker when using in higher than 40 DEG C ambient temperatures ?

Product:
MTZ Breaker

Environment:
Application

Cause:
Product Features

Resolution:
The MTZ breaker can operate within -25 DEG C to + 70DEG C temperature range and a re-rating multiplier needs to be applied with higher than 40 DEG C per the ANSI temperature re-rating Chart .
For example:
+ 40 DEG C ambient =100% rated Amps
+50 DEG C ambient = 92%  rated amps. This would calculate out for example, to a 1000A trip sensor X .92 derating factor equaling a real trip amperage of 920A .

Schneider Electric USA