{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the part number for extra straps that can be used with the Strap On ETS 800 thermistor sensor?

Issue:
Are extra straps available for the ETS800 sensors to fit larger than 5" diameter pipe?

Product:
Sensors / Thermostats

Environment:
Installation

Cause:
Installing on larger diameter Pipe

Resolution:
These straps are no more than worm gear tightening hose clamps and can be bought at local Hardware, or Automotive Stores. Adding length is easily done by inserting one end of the additional hose clamp (Strap) into the backside of ETS800 strap. Using the worm gear screw of the ETS800 strap, turn the screw to draw the addtional strap into it. This will add extra length to the sensor strap, which will then allow the sensor to be mounted to the larger diameter Pipe.

See the ACI attachment with options as well as the ETS 800 Bulletin.

Schneider Electric USA

Attachment(s)
ETS 800 Thermistors Strap On.pdf [334.11 KB]
ET Sensors F-27601-6.pdf [783.12 KB]