{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Is there an alternative to the Barber Colman DVAV-3 stepper motor?
Issue:
What is the cross for the DVAV-3 Stepper motor ?

Product:
Stepper Motors

Environment:
Maintenance

Cause:
Replacement

Resolution:
The DVAV-3 Stepper motors are obsolete with no replacement . They were originally supplied by the Crouzet Co. as part number 82-910-029 , see attached dwg.
There are suppliers that possibly would have this On Line , HVAC Plus for example

Schneider Electric USA

Attachment(s)
DVAV.docx [44.09 KB]