{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the packing cartridge for a VB-7211 valve body
Issue:
Is there a packing kit for the VB-7211-0-4-XX valves?

Product:
Valves and Actuators

Environment:
Maintenance

Cause:
Repair/ Replacement

Resolution:

The replacement packing cartridge is part number YBA-622-2 .

** The YBA-622-2 was not designed to be used to repair VB-131, VB-151, 1/2" VB-922x, -9263, or -9283 valves, or 1-1/2" to 2" VB-9xxx valves.**
See Instruction Bulletin attached

Schneider Electric USA

Attachment(s)
YBA-622 YBA-635 F-17324-11.pdf [94.89 KB]