{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the input voltage range for the BMXDAI1604?
Issue
The module is specified as 100... 120VAC, is that the absolute full range?

Product line
Modicon X80 IO

Resolution
The specified sensor operating range for the BMXDAI1604 module is 85... 132V.

The input ON is at >= 74V, 2.5MA
The input OFF is at <= 20V, 1mA


If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric USA

Explore more
Range:
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Product: