Issue:
RIM module for MTZ and Series B trip unit
Product Line:
Circuit Breakers
Resolution:
The MTZ RIM module LV848892SP will support series B upstream only. To support Series B downstream they need one of the following:
S48890 (120 Vac/24 Vdc)
S48895 (240 Vac/24 Vdc)
RIM module for MTZ and Series B trip unit
Product Line:
Circuit Breakers
Resolution:
The MTZ RIM module LV848892SP will support series B upstream only. To support Series B downstream they need one of the following:
S48890 (120 Vac/24 Vdc)
S48895 (240 Vac/24 Vdc)
Released for:Schneider Electric USA