{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Is a handle extension available for the Powerpact R frame breaker?
Issue:
Add extra leverage to turn breaker off or on

Product Line:
PowerPact R

Resolution:
No handle extensions are available for the R frame breaker. The only handle is the standard which can be replaced. The part number for replacement is S33997.

Schneider Electric USA