{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Can Unity Pro be set up with user access rights control?
Issue
Is it possible to create User profiles for Unity Pro or EcoStruxure Control Expert so that depending on which login is used it has different permissions?

Product line
Unity Pro, Control Expert

Resolution
User profiles can be set up for Unity Pro. This needs to be set up in the Security Editor. The Security Editor can be found in the default Unity Pro install directory along side the PLC Simulator, Exec Loader , etc.  When you launch the Security Editor you will be prompted for a Username/Password;
The default for Unity Pro/ECE <= v15.1 is Supervisor for username with no password (Enter).
The default for ECE v15.2 and v15.3 is SecurityAdmin for username and password Azertyuiop12!
The default for ECE v15.3 with HF7 and v16.0 is SecurityAdmin for username and password Azertyuiop123456789!

Schneider Electric USA