{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Does Schneider Electric build transformers per impedance requirements?
Issue:
Impedance being part of the requirements

Product Line:
Transformers

Environment:
Special/custom Build Products

Resolution:
Impedance is not a target attribute for our designs, like efficiency and low heat contribution are.  The impedance is the result of a design, not the end goal. But it will be within the proper range based on the Nema Standards below:
 
Nema Standards for Transformer Impedance
Transformer Capacity% Impedance
15 to 150 kVA1.5 to 6.0
225 to 300 kVA3.0 to 7.0
500 kVA4.5 to 8.0
750 kVA5.0 to 8.0
*margin of error is +/-7.5%

 

Schneider Electric USA

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.