{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
How is a MP-5413 actuator wired?
Issue:
What does the Red , Yellow and Blue wires connect to on a MP-5413 actuator?

Product:
Valves and Actuators

Environment:
Installation

Cause:
Wiring

Resolution:
That 24VAC Power is wired to Blue/ Black and Black is Com. Red , if needed, is for + 20VDC supplied by the actuator for the upstream Thermostat. Yellow is connected from the stats 6-9 VDC Control signal and Blue is the Common.
Note the Red +20VDC lead is power produced by the actuator's internal transformer for power to the Thermostat, if not needed , tape off.
Actuator wiring

Schneider Electric USA

Attachment(s)
MP-5400 Act F-24788.pdf [871.03 KB]