{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Does Schneider endorse the use of pin or mac adapters on circuit breakers?
Issue:
Does Schneider approve of pigtail or mac adapters to reduce large cable to fit in circuit breaker lugs?

Product Line:
Circuit Breakers

Environment:
All MCCB with cable connections

Resolution:
Schneider has not tested or validated these adapters (pin, mac, cop, etc.) for use with circuit breakers and so cannot endorse their use.
Lugs are tested with and are rated for stranded wire only. Adapters with stranded pins or pigtails simulating stranded wire will affect wire-bending space and it is up to the AHJ (local inspector) as to whether or not they're allowed.
Alternate mechanical lugs and optional compression lugs identified for the breaker should also be considered as these sometimes allow larger wire sizes than the standard lugs.

Schneider Electric USA

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.