{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What torque should be applied to the X1 and X2 terminals on the MDGF (Modified Differential Ground Fault) sensors S33579?
Issue:
There is no torque specification supplied with the S33579 sensor or MDGF instructions for terminals X1 and X2.  (SE internal part number 63103-038-63)

Product Line: Circuit Breakers
Environment: MDGF system

Resolution:
The torque recommendation is 25 in. lbs.

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: