{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Can a tandem breaker be used in an NQOD or NQ panel?
Issue:
Are tandem breakers suitable to be used in NQOD or NQ panelboards?

Product Line:
Load center tandem breakers

Environment:
QOT

Resolution
No. The tandem breaker is designed for specific, residential  QO  load center applications only. Tandem breakers are not UL tested or certified for use in panelboards

Schneider Electric USA