{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Can I use two cables per lug on an LA/LH type breaker?
Issue:
Can I use two cables per lug on an LA or LAL breaker?

Product Line:
Circuit Breakers

Resolution:
Yes. The standard lug is AL400LA. It has been tested and UL listed for two cables per pole, up to 250 kcmil. Some inspectors may tell you it cannot be used, but they are incorrect. It may be applied as listed.

Schneider Electric USA