{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Need a 30mm pushbutton with push-on push-off operation.
Issue:
What is the Push-on, Push-off Module to use with 9001 Type K, KX, SK or T momentary push button operators?

Product Line:
Harmony 30 mm 9001 K Metal Push Buttons

Environment:
30mm Push Buttons

Resolution:
Use a standard 9001 Type K momentary operator and the 9001 K85 push-on push-off module. Any contact blocks mounted behind the module will operate as push-on push-off. Any contacts mounted in tandem will remain momentary.

Schneider Electric USA

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: