{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Are solid neutral assemblies available for ALL heavy duty safety switches? What neutral is used with each switch and what is the terminal lug data?
Issue:
Product Design Features

Product Line:
Heavy Duty Safety Switches

Resolution:
All heavy duty switches will accept a solid neutral assembly with some exceptions. SEE the below solid neutral table and select the neutral based on the amperage of the switch.
NOTES:
1) LOOK AT ALL APPROPRIATE FOOTNOTES UNDER THE TABLE

2) A solid neutral CANNOT be added to the H364DF and HU364DF (NEMA 4X fiberglass reinforced polyester)
3) For older series switches, SEE SWITCH WIRING DIAGRAM

Neutral table
[65] For series not shown in chart refer to the switch wiring diagram
[67] For solid Neutral Assembly Kits for Krydon TM enclosure see Table 3.20 Below.
[68] For Solid Neutral Assembly Kits for Fiberglass Reinforced Ployester enclosures see Table 3.19 Below.
[69] Neutrals CANNOT be installed in 4 or 6 pole switches or Receptable Switches.
[70] See Current ON-LINE Digest or Switch wiring diagram for Current Series of Safety Switch.
[71] The following 30 A Series F5-F6 switches use SN0610 or SN0610C: H3612, H3612RB, H3612A, H3612AWK, HU3612, HU3612RB, HU3612A and HU3612AWK.
[72] For 200% neutral, order (2) SN20A Neutral Kits and (1) SN20NI Neutral Jumper Kit (THIS ONLY APPLIES TO THE 200Amp SWITCHES)
Neutral table 2

Schneider Electric USA