{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Video: What is the difference between a ring type and a ringless type meter socket?
Issue:
Differentiating Ring Type & Ringless Meter Sockets

Product Line:
Meter-Pak, Combination Service Entrance Devices, EZ Metering, Individual Meter sockets

Resolution:
The ring type meter cover has a formed rim on the cover which works with a sealing ring to directly seal the meter in place. The ringless type meter cover has a draw in the cover that fits over the meter and holds the meter in place and the cover can be sealed or padlocked with the hasp on the cover.

Schneider Electric USA

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
move-arrow-top