{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Can I-Line panels be ordered with a neutral?
Issue:
Does a neutral assembly have to be ordered separately from the I-Line panel interior?

Product Line:
Panelboards

Environment:
I-Line panelboards and accessories.

Resolution:
The following interiors are provided with a neutral as standard:

225A  HCM
1200A HCP

The interior catalog numbers that include a neutral have the suffix "N" after the catalog number.  Otherwise, the neutral must be ordered separately. Reference the
current Digest, Section 9 for selection .

The catalog number listed in the Digest has an N at the end. (Example: HCP508612N)

Schneider Electric USA