Issue:
Identify if 8941 duplex controllers are available for single-phase applications
Product Line:
Class 8941 Duplex Motor controllers
Environment:
Motor Starters
Cause:
Product Selection
Resolution:
Yes, select it appropriately per NEMA size required for single-phase motor voltage and horsepower rating. Add form Y177 to have the factory rewire it for single-phase applications. This form has no price adder. Solid state overload relays cannot be selected for single phase applications.
Released for:Schneider Electric USA