{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the replacement lever arm and float guide for the 9036DW31?
Issue:
Replacement Lever Arm for 9036DW31.

Product Line:
Pressure Switch and Float Switch

Environment:
Open Tank Types D and G

Resolution:
Part # is 65079-034-01 for single piece device. For devices having a 2 piece lever, or as a substitute, use 1546-L15-X1 for the lever, and 1091-S18-G6 for the guide that bolts to the lever.
See the attached file.

Schneider Electric USA

Attachment(s)
9049 - A6_.pdf [24.87 KB]