{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the float for a 9036DR31?
Issue:
Float kit for 9036DR31

Product Line:
Float Switch

Environment:
Kits for Class 9012–9038 Devices

Resolution:
Recommended float will be a center hole device. A float kit, including rod and stops, is normally required for initial installation. Choose from 9049 A6C or A6CA or A6CS. Once the initial installation is complete, replacement floats would be 9049AF1 6507300251 ( #304 stainless type) or 9049AF2 6507300253 (#316 stainless type).

Schneider Electric USA